Part Number: TMDSDOCK28335
Other Parts Discussed in Thread: CONTROLSUITE
Hi Team,
Need your expertise on our customer's query. They intend to simulate their control system using the TMDSDOCK28335 control card on the OPAL-RT simulator platform. And they'd like to know how to send and receive information between target simulator and the TMDSDOCK28335 controller using CAN connection.
They've already looked at the sample codes given in Controlsuite and ran across some questions. Can you help us with the resources or documentation references that they could read on to address these?
1. How does the E-CAN example works? what are the data that they are trying to send? (eCAN-A to eCAN-B Transmit Loop (ecan_a_to_b_xmit)).
2. I need to know the following items in that example:
- Type of the data
- Start bit
- Size
- Is there any initial value and max or min values
Thanks in advance!
Kind Regards,
Jejomar