Part Number: TMS320F28388S
Hi,
I have a question about the EMIF1.
In the datasheet, it states that the CS for EMIF1 for asynchronous memory is EMIF_CS[4:2].
when I looked on the memory map of the CS I saw the following note:
"Dual Map - When EMIF1 CS0n is mapped at address 0x2x_xxxx, EMIF1 CS2n is only available from 0x10_0000 to 0x1F_FFFF (1M x
16)."
I looked in the TRM if there is anything to support this note. but found nothing. Can I use the CS0n for asynchronous memory?
I want to use the CS0 because I actually need two CS with 1Mx16 size.
Thanks,
Tal