Part Number: TMS320F280049C
Hello TI,
first is it possible to configure the DMA that he takes samples of SOCs0,2,4,6,8 ...
I am using the burst mode to sample higher frequent signals on even SOCs and lower frequent signals on the odd SOCs.
I have 3 high frequent signals which should fill a buffer of 1000 samples. In order to reduce load, using the the samples out of the result buffer would probably help.
If this is possible, is there an example?
Best Regards