This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280025: bitwise operation example code for CAN module

Part Number: TMS320F280025
Other Parts Discussed in Thread: C2000WARE

Hi,

my customer is migrating their code from F2803x to F28002x, so they ask if we could provide bitwise operation example code for CAN module. They are not used to the driverlib example.

  • Hi,

    They can refer to bit field examples for device F2837xd at location C2000Ware_3_04_00_00\device_support\f2837xd\examples\cpu1\can_loopback_interrupts\cpu01. Other than header and pin mux configuration most of it should be similar. 

    For a projectspec reference they can refer to existing bit filed examples for f28002x at C2000Ware_3_04_00_00\device_support\f28002x\examples

    Regards,

    Yashwant