Other Parts Discussed in Thread: CONTROLSUITE, TINA-TI
I have a F28377D controlcard with the docking station and i have start to test the ADC modules by measuring known voltage from a power supply. However in the AdcResultRegs i get the same value for small changes on the voltage and i have to change the voltage fairly much to get a new value in the register, about 0.3V perhaps. Worth to notice is that the values in the register doesnt increase linearly when i change the voltage on the power supply, it seems to increase very fast between 0.5V and 2V and between that it doesnt change much at atll.
I have single ended conversion 12 bit resolution, like 50 clock cycles aquisition window and the switches on the hardware are set to use an external reference on the controlcard which should be 3.3V according to documentation. If you need more info or a part of the ADC initalization code i can provide that.
/Kristoffer