This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

error #10234-D: unresolved symbols remain error #10010: errors encountered during linking; "TIMER0.out" not built

你好,我用的是dsp28335,ccsv6版本,调试的程序是用定时器终端控制流水灯。但是编译程序的时候,出现上面的错误。这是工程的设置以及程序。

#include "DSP2833x_Device.h" // DSP2833x Headerfile Include File
#include "DSP2833x_Examples.h" // DSP2833x Examples Include File


#define LED1 GpioDataRegs.GPADAT.bit.GPIO0
#define LED2 GpioDataRegs.GPADAT.bit.GPIO1
#define LED3 GpioDataRegs.GPADAT.bit.GPIO2
#define LED4 GpioDataRegs.GPADAT.bit.GPIO3
#define LED5 GpioDataRegs.GPADAT.bit.GPIO4
#define LED6 GpioDataRegs.GPADAT.bit.GPIO5


interrupt void ISRTimer0(void);
void configtestled(void);


void main(void)
{
// Step 1. Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks
// This example function is found in the DSP2833x_SysCtrl.c file.
InitSysCtrl();

// Step 2. Initalize GPIO:
// This example function is found in the DSP2833x_Gpio.c file and
// illustrates how to set the GPIO to it's default state.
// InitGpio(); // Skipped for this example
InitXintf16Gpio(); //zq

// Step 3. Clear all interrupts and initialize PIE vector table:
// Disable CPU interrupts
DINT;

// Initialize the PIE control registers to their default state.
// The default state is all PIE interrupts disabled and flags
// are cleared.
// This function is found in the DSP2833x_PieCtrl.c file.
InitPieCtrl();

// Disable CPU interrupts and clear all CPU interrupt flags:
IER = 0x0000;
IFR = 0x0000;

// PIE 向量表指针指向中断服务程(ISR)完成其初始化.
// 即使在程序里不需要使用中断功能,也要对 PIE 向量表进行初始化.
// 这样做是为了避免PIE引起的错误.
// The shell ISR routines are found in DSP2833x_DefaultIsr.c.
// This function is found in DSP2833x_PieVect.c.
InitPieVectTable();

// Interrupts that are used in this example are re-mapped to
// ISR functions found within this file.
EALLOW; // This is needed to write to EALLOW protected registers
PieVectTable.TINT0 = &ISRTimer0;
//PieVectTable.XINT13 = &cpu_timer1_isr;
//PieVectTable.TINT2 = &cpu_timer2_isr;
EDIS; // This is needed to disable write to EALLOW protected registers

// Step 4. Initialize the Device Peripheral. This function can be
// found in DSP2833x_CpuTimers.c
InitCpuTimers(); // For this example, only initialize the Cpu Timers

// Configure CPU-Timer 0, 1, and 2 to interrupt every second:
// 150MHz CPU Freq, 1 second Period (in uSeconds)

ConfigCpuTimer(&CpuTimer0, 150, 500000);
//ConfigCpuTimer(&CpuTimer1, 150, 1000000);
//ConfigCpuTimer(&CpuTimer2, 150, 1000000);
StartCpuTimer0();

// Enable CPU int1 which is connected to CPU-Timer 0, CPU int13
// which is connected to CPU-Timer 1, and CPU int 14, which is connected
// to CPU-Timer 2:
IER |= M_INT1;
//IER |= M_INT13;
//IER |= M_INT14;

// Enable TINT0 in the PIE: Group 1 interrupt 7
PieCtrlRegs.PIECTRL.bit.ENPIE = 1;
PieCtrlRegs.PIEIER1.bit.INTx7 = 1;

// Enable global Interrupts and higher priority real-time debug events:
EINT; // 总中断 INTM 使能
ERTM; // 使能总实时中断 DBGM
configtestled();
LED1=0;
DELAY_US(10);
LED2=0;
DELAY_US(10);
LED3=0;
DELAY_US(10);
LED4=0;
DELAY_US(10);
LED5=0;
DELAY_US(10);
LED6=0;
DELAY_US(10);

for(; ;)
{
}

}


interrupt void ISRTimer0(void)
{
CpuTimer0.InterruptCount++;

// Acknowledge this interrupt to receive more interrupts from group 1
PieCtrlRegs.PIEACK.all = PIEACK_GROUP1; //0x0001赋给12组中断ACKnowledge寄存器,对其全部清除,不接受其他中断
CpuTimer0Regs.TCR.bit.TIF=1; // 定时到了指定时间,标志位置位,清除标志
CpuTimer0Regs.TCR.bit.TRB=1; // 重载Timer0的定时数据

LED1=~LED1;
LED2=~LED2;
LED3=~LED3;
LED4=~LED4;
LED5=~LED5;
LED6=~LED6;



}

void configtestled(void)
{
EALLOW;
GpioCtrlRegs.GPAMUX1.bit.GPIO0 = 0; // GPIO0 = GPIO0
GpioCtrlRegs.GPADIR.bit.GPIO0 = 1;
GpioCtrlRegs.GPAMUX1.bit.GPIO1 = 0; // GPIO1 = GPIO1
GpioCtrlRegs.GPADIR.bit.GPIO1 = 1;
GpioCtrlRegs.GPAMUX1.bit.GPIO2 = 0; // GPIO2 = GPIO2
GpioCtrlRegs.GPADIR.bit.GPIO2 = 1;
GpioCtrlRegs.GPAMUX1.bit.GPIO3 = 0; // GPIO3 = GPIO3
GpioCtrlRegs.GPADIR.bit.GPIO3 = 1;
GpioCtrlRegs.GPAMUX1.bit.GPIO4 = 0; // GPIO4 = GPIO4
GpioCtrlRegs.GPADIR.bit.GPIO4 = 1;
GpioCtrlRegs.GPAMUX1.bit.GPIO5 = 0; // GPIO5 = GPIO5
GpioCtrlRegs.GPADIR.bit.GPIO5 = 1;

EDIS;
}

//===========================================================================
// No more.
//===========================================================================

  • 哈哈,居然用中文。
  • 你好,

    下面的回复请使用英文,方便美国专家理解你的问题并提供建议。

    我想请问的是,你程序里unresolved symbols中的symbols究竟是哪个symbol?

    你可以将编译时下方console窗口里的相关内容(特别是红色标注的部分)截取出来,或者全选后拷贝发出来,然后可以根据这个信息去搜索你的程序中与这个symbol相关的代码,找到问题所在。

     

    Hello,

    Please use English to reply in your next post, which will be helpful for U.S. expert to understand your question and give you suggestions.

    My question is, which symbol exactly is it in your project when it reported "unresolved symbols".

    You can simply captured related contents in the console window (especially red indicated session) when compiled or select all and then copy entire compile information to post it here, and then you can search your project to find all codes where the symbols are existed to find the root cause.

     

    Best Regards,

    Ricky Zhang

  • hello
    just now。 I had same problem 。the solution is an follow, I hope that will be helpful. find project-right click the mouse-click properties-build-Advanced Options-Symbol Management (Delete code-strat),OK, it wll successful. I love the Chinese!