Hi there,
I have been trying the CLA with Example_2805xClaAdc on a F28055 and have found that CLA isn't running at all; it will not stop at the break point I set at CLA ISR, nor the variable, ConversionCount, will increase and then reset. However, when I try the same sample code on a brand new board, everything works fine. These two boards are identical, but I previously enabled DCSM on the old board. Does DCSM has anything to do with CLA not running? If so, how can I get CLA to work on the device whose DCSM was once enabled?
Thank you
regards,
Kevin