This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to GET RX PARAMETER (SNR/NL/RQ..) on PHY_G3_EXAMPLE

Hi everyone,

I'm trying to modify the code PHY_G3_EXAMPLE to acquire some data as SNR, Reception Quality etc.

I have some trouble to understand how does the PHY_rxGet(UINT16 getType, UINT16 *getData_p) works. I have implemented this function inside the code by first declaring the structure -> PHY_rxGetData_t rxget and then recall the PHY_rxGet function for example in this way:

-PHY_rxGet(PHY_RX_GET_TONEMAP_INFO,&rxget);

val10=rxget.toneMapInfo;

-PHY_rxGet(PHY_RX_GET_NL,&rxget);

val7=rxget.nl;  etc...

The problem is that when I look the variables: val10, val7 (that I have declared before as UIN16) the result is 0. Only If I put inside the function "PHY_RX_GET_TONEMASK" correspond with the TX value, but for example if I want to know the SNR (so I put inside the function "PHY_RX_GET_SNR" ) or other parameter (as NoiseLevel, sb_SNR, ReceptionQuality..) the value is always 0.

Can someone tell me the reason?

Thanks for your support,


Best,

Andrea

  • Hi Andrea,

    Can you explain when/where do you call PHY_rxGet(..) ?
    I hope you have a working setup where you see TX and RX packets sent and received over power line?

    So, do you see that val10 gets the value sometimes or never?

    Thanks,
    Katta
  • Hi Katta,

    Thanks for replying.

    I call PHY_rxGet(..) in the main.c, precisely in that part of the code:

    void cb_ppdu(PHY_ev_t eventID, PHY_cbData_t *cbData_p)
    {

      if (cbData_p->status == PHY_STAT_SUCCESS)
        {............}


    That mean, each time a packet arrives and a GPIO LED blink.

    I tried also to create a function:

    void getvalue(void) {

    PHY_rxGetData_t rxget;

    PHY_rxGet(PHY_RX_GET_RQ,&rxget);

    val12=rxget.rq;

    PHY_rxGet(PHY_RX_GET_SNR,&rxget);
    val10=rxget.snr;

    PHY_rxGet(PHY_RX_GET_NL,&rxget);
     val11=rxget.nl;

    .......... }

    that is called every 1second from PRD DSP BIOS but the problem is that the NOISE LEVEL, RECEPTION QUALITY, SNR, SINGLE_SBN_SNR are always zero, others values in PHY_rxGet(..) (as TONE_MASK) are right and different from zero.

    I hope for your support.

    Best,

    Andrea

  • Hi Andrea,

    On this setup did you ran PHY Performance test?
    It is explained in 'TI G3 User Guide-Zero Config GUI.pdf' 2.9 section.

    Please check if you see the statistics(ex:- SNR, RSSI, PER, BER) change.
    The 'number of packets detected' should increase and header failures should be zero.
    This test is to ensure your setup is working.

    Or else monitor 'phyRxPpduCount' value in your code. It should be a non-zero value.

    In your current setup how do you make sure the transmission and reception are happening?

    Thanks,
    Katta
  • Hi Katta,

    I'm not using the "Zero Configuration GUI" but my own program based on the G3_PHY_EXAMPLE.

    Everything works well: the TX TMDPLCKIT-V3 send a packet every 1second and the RX TMDPLCKIT-V3 receive that packet and blink a LED.

    I'd like to acquire the parameters: SNR, SBN_SNR, NL, RQ and I thought that was enough to call the function in my RX_code.

    The other statistics, as I mentioned before, works. For example, using phyRxPpduCount, I see that the value increase.

    If you want, I can send my modified code so you can take a look.


    Thanks a lot in advance,

    Andrea

  • I post here a part of the code and what display at the output:

    As you can see the values of: RQ, SB.SNR, NOISE LEVEL, are incorrect. Here I created a function that every second launch the PHY_rxGet(..) and it could acquire the desired data.

    I hope that is more clear now,

    Thanks,

    Andrea

  • Hi Andrea,

    I have two suggestions.
    1. Are you looking at the values with the system running or paused at a breakpoint. From the image it appears the system is running. Can you pause and check?
    2. Instead of looking for the values at each second with a breakpoint, try to save the values to a buffer over a period of 1 min and look whether the values were non-zeroes any time.

    We too use similar code. It works on our setup. The Zero configuration GUI uses same mechanism to show these values.

    Thanks,
    Katta
  • Hi Katta,

    1) Yes, the system is running. However I tried to stop the system with a breakpoint but the values are the same.
    From a certain point of view, val10 that is my SNR is correct (because it has to reach values from 0 to 7) , I have 5.

    But the other values for example val12, that is my ReceptionQuality has the value 48680 that is wrong because on phy_rx.h is write:

      UINT16          rq;          // receive quality (0 to 8 from bad to good)"

    2) I tried also to save the values in a buffer but the results are more or less the same.

    My guess it that is like is missing some convertion or format number for the other parameters.

    I hope again for your support,

    Andrea

  • I attach here my RX main.c so you can take a look.

    The program, in a few word, blink the LED everytime a packet in sent from the TX TMDSPLCKIT-V3.

    I hope it can help you to understand better,


    Best,


    Andrea

    /******************************************************************************
    * FILE PURPOSE: This file implements the G3 PHY TX/RX Test
    *******************************************************************************
    *
    * FILE NAME: test_tx_rx.c
    *
    *
    ******************************************************************************/
    /* configuration file */
    #ifdef F2806X
      #include <test_tx_rx_f2806xcfg.h>
    #elif defined (F28M35X)
      #include <test_tx_rx_f28m35xcfg.h>
    #else
      #include <test_tx_rxcfg.h>
    #endif
    
    #include "DSP28x_Project.h"
    
    #include <phy_rx.h>
    #include <phy_tx.h>
    #include <phy_test.h>
    #include <hal_afe.h>
    #include <phy_tx_swi.h>
    
    #define VETTORE_LENG  1
    #define PHY_RX_BUF_SIZE 10
    
    int16 line_buffer[VETTORE_LENG];
    int16 rx_ppduBuf[PHY_RX_BUF_SIZE];
    
    UINT16 getCRC8(uint16 input_crc8_accum, uint16 *msg, parity_t parity, uint16 rxLen);
    UINT16 getCRC8_vcu_asm(uint32 input_crc8_accum, uint16 *msg, parity_t parity, uint16 rxLen);
    
    //VARIABLES
    UINT16 val1,val2,val3,val4,val5,val6,val7,val8,*valp1,val9[24], val10,val11,val12,val13,val14,snr,quality;
    
    UINT32 cnt;
    PHY_rxAagcGet_t agc;
    PHY_rxCdGet_t cd;
    PHY_rxToneMask_t tm;
    
    void ledBlink_gpio31();
    void Setup_eCAP1(void);
    void eCAP1_isr(void);
    
    
    
    PHY_txSetData_t test_toneMask_s =
    
    {
      0x2417,//2417 18- 24 sub carriers 01- start tone 1*1,5625 kHz = 1,5625 kHz
      0xFFFF,//FFFF
      0xFFFF,//FFFF
      0x000F,//000F
      0x0000,//0000
      0x0000,//0000
      0x0000//0000
    };
    
    
    //Receiver Gain
    PHY_rxAagcSet_t agc_gain_s =
    {
    	0,//0-auto 1-manual
    	//7//0-7 step 6dB
    };
    
    
    void flash_setup(void);
    void sys_init_phy_rx(void);
    void sys_init_phy_tx(void);
    void PHY_tx_sema_post();
    void get_tutto();
    
    
    extern void cb_bit(PHY_ev_t eventID, PHY_cbData_t *cbData_p);
    void cb_ppdu(PHY_ev_t eventID, PHY_cbData_t *cbData_p);
    
    UINT32 idle_cnt=0;
    #ifdef P1901_2_FCC
     UINT32 test_toneMap = 0xFFFFFF;
    #else
     UINT32 test_toneMap = 0x003F;//3F 1bit presents 6 tones (sub carriers)
    #endif
    UINT16 test_toneCoef[2] = {0x0000, 0x0000};//each 4-bit field is 2-compliment gain
    
    /******************************************************************************
    * FUNCTION NAME: sys_init
    *
    * DESCRIPTION:
    
    ******************************************************************************/
    void sys_init_hw(void)
    {
      // Step 1. Initialize System Control:
      // PLL, WatchDog, enable Peripheral Clocks
      // This example function is found in the DSP2833x_SysCtrl.c file.
    
      DINT;     // Global Disable all Interrupts
      IER = 0x0000;         // Disable CPU interrupts
      IFR = 0x0000;         // Clear all CPU interrupt flags
    
      // Step 1. Initialize System Control:
      // PLL, WatchDog, enable Peripheral Clocks
      // This example function is found in the DSP2833x_SysCtrl.c file.
      InitSysCtrl();
      Setup_eCAP1();		// init  eCAP1
    
      /* Map ePWM registers to PF3 */
      EALLOW;
    //  SysCtrlRegs.MAPCNF.bit.MAPEPWM = 1;
      EDIS;
    
      // Step 1a. Reset peripherals
      DMAInitialize();
    
      // RLiang TX-PHY need this one
      InitCpuTimers();
    
      // Specific clock setting for this example:
      //EALLOW;
      //SysCtrlRegs.HISPCP.all = ADC_MODCLK;    // HSPCLK = SYSCLKOUT/ADC_MODCLK
      //EDIS;
    
      // Step 2. Initialize GPIO:
      // This example function is found in the DSP2833x_Gpio.c file and
      // illustrates how to set the GPIO to it's default state.
      // InitGpio();  // Skipped for this example
    
      // Step 3. Clear all interrupts and initialize PIE vector table:
      // Disable CPU interrupts
      DINT;
    
      // Initialize the PIE control registers to their default state.
      // The default state is all PIE interrupts disabled and flags
      // are cleared.
      // This function is found in the DSP2833x_PieCtrl.c file.
      InitPieCtrl();
    
      // Disable CPU interrupts and clear all CPU interrupt flags:
      IER = 0x0000;
      IFR = 0x0000;
    
      // Initialize the PIE vector table with pointers to the shell Interrupt
      // Service Routines (ISR).
      // This will populate the entire table, even if the interrupt
      // is not used in this example.  This is useful for debug purposes.
      // The shell ISR routines are found in DSP2833x_DefaultIsr.c.
      // This function is found in DSP2833x_PieVect.c.
      InitPieVectTable();
    	PieCtrlRegs.PIEIER4.bit.INTx1 = 1;	// Enable ECAP1_INT in PIE group 4
    	IER |= 0x0009;						// Enable INT4 and INT1
    
    
      // Enable global Interrupts and higher priority real-time debug events:
         EINT;   // Enable Global interrupt INTM
         ERTM;   // Enable Global realtime interrupt DBGM
    }
    
    /***********************************************************************/
    /* Call back for PHY_rxPpdu BitDone                                           */
    /***********************************************************************/
    
    void cb_ppdu(PHY_ev_t eventID, PHY_cbData_t *cbData_p)
    {
    
      if (cbData_p->status == PHY_STAT_SUCCESS)
        {
    	  int i;
    	  PHY_rxPpdu_t * rxppdu = (PHY_rxPpdu_t *)(cbData_p->cbParms.rxPpdu.ppduInfoAddr);  	// pointer a date
    	  int *data = (int *)rxppdu->data_p;
    	  PHY_rxPpduRelease(rxppdu);
    
    	  //BLINK LED EVERYTIME PACKET ARRIVES//
          GpioDataRegs.GPATOGGLE.bit.GPIO31 = 1;
        }
    }
    
    
    
    /******************************************************************************
    * FUNCTION NAME: main
    
    ******************************************************************************/
    void main(Void)
    {
    
      HAL_afe_prfParms_t afePrfParms;
      PHY_rxPpdu_t PHY_rx_ppdu_s;
      /* initialize HW */
      sys_init_hw();
    
      /* setup for flash */
      flash_setup();
    
      /* init LED */
      //LED_init();
    
      EALLOW;
    
      GpioCtrlRegs.GPBMUX1.bit.GPIO34 = 0; //0-GPIO
      GpioCtrlRegs.GPBDIR.bit.GPIO34 = 1; //1-output
      GpioCtrlRegs.GPAMUX2.bit.GPIO31 = 0; //0-GPIO
      GpioCtrlRegs.GPADIR.bit.GPIO31 = 1; //1-output
      GpioCtrlRegs.GPAMUX1.bit.GPIO6 = 0; //0-GPIO
      GpioCtrlRegs.GPADIR.bit.GPIO6 = 1; //1-output
      GpioCtrlRegs.GPAMUX1.bit.GPIO7 = 0; //0-GPIO
      GpioCtrlRegs.GPADIR.bit.GPIO7 = 1; //1-output
      GpioCtrlRegs.GPAMUX1.bit.GPIO8 = 0; //0-GPIO
      GpioCtrlRegs.GPADIR.bit.GPIO8 = 1; //1-output
    
      /* HAL profile (tx/rx sampling and PWM frequencies */
    #ifdef AFE031
        /* AFE031 requires 3x TX sampling rate */
        afePrfParms.tx_fs_kHz = HAL_AFE_KHZ_1200;//1200
    #else
      afePrfParms.rx_fs_kHz = HAL_AFE_KHZ_400;//400
      afePrfParms.tx_fs_kHz = HAL_AFE_KHZ_400;//400
      afePrfParms.tx_pwm_kHz = HAL_AFE_KHZ_1200;//1200
    #endif
    
    #if defined(CENELEC_B) || defined(CENELEC_BC)
      afePrfParms.band = 1;
    #else
      afePrfParms.band = 0;
    #endif
    
      HAL_afeInit(&afePrfParms);
    
      /* init PHY Rx */
      sys_init_phy_rx();
    
      /* init PHY TX */
      sys_init_phy_tx();
    
      /* Set tonemask */
      PHY_rxSet(PHY_RX_SET_TONEMASK, (PHY_rxSetData_t *)&test_toneMask_s);
      PHY_rxSet(PHY_RX_SET_AGC, (PHY_rxSetData_t *)&agc_gain_s);
    
    
      // initialize PHY band and reconfigure the afe parameters
      PHY_init();
    
      PHY_rx_ppdu_s.data_p = (Uint16 *)&rx_ppduBuf[0];
    
      /* Start PHY Rx */
      PHY_rxStart(0xFFFF, cb_ppdu);
    
      /* Register for bit start */
      PHY_rxBitStartIndicate(cb_bit);
    
      /* enable sys interrupt */
      EnableInterrupts();
    
    }
    
    
    Uint32 blinkCnt=0;
    void ledBlink_gpio31()
    {
    #ifdef F28M35X
       // silicon errata: sprz357.pdf
       if(GpioG1DataRegs.GPCDAT.bit.GPIO71 == 0){
       	 GpioG1DataRegs.GPCSET.bit.GPIO71 = 1;
       }else{
       	 GpioG1DataRegs.GPCCLEAR.bit.GPIO71 = 1;
       }
    #else
        GpioDataRegs.GPBTOGGLE.bit.GPIO34 = 1;
    #endif
      blinkCnt++;
    }
    
    
    void get_all(void){
    	int i;
    	/*I can call this function from DSP BIOS PRD EVERY SECOND (for example) Or put All this stuff inside the callback when BLINK THE LED
    	 * BUT THE RESULTS IS THE SAME, SNR WORK BUT OTHER VARIABLES NOT
    	 */
    	//STATISTICS
    		  		PHY_rx_stat_t rxstats;
    		  		PHY_rxGetStat(&rxstats);
    		  		val1=rxstats.phyAgcStepNum;
    		  		val2=rxstats.phyAgcStepValue;
    		  		val3=rxstats.phyCrcFailCount;
    		  		val4=rxstats.phyRxDropCount;
    		  		val5=rxstats.phyRxQueueLen;
    		  		val6=rxstats.phyCrcIncorrectCount;
    		  		cnt=rxstats.phyRxPpduCount;
        //....
    		  	PHY_rxGetData_t rxget;
    		  	PHY_rxGet(4,&rxget); //I PUT HERE "4" BUT IS THE SAME IF I COPY THE PHY_RX_RQ ON PHY_RX.H"
    		    val12=rxget.rq;
    		    PHY_rxGet(PHY_RX_GET_TONEMASK,&rxget);
    		  	tm=rxget.toneMask;
    		    PHY_rxGet(PHY_RX_GET_SNR,&rxget);
    		  	val10=rxget.snr;
    		  	PHY_rxGet(PHY_RX_GET_NL,&rxget);
    		  	val11=rxget.nl;
    
    }
    
    // CRC8 convertion function
    uint16 getCRC8 (uint16 input_crc8_accum, uint16 * msg, parity_t parity,
        uint16 rxLen)
    {
      return getCRC8_vcu_asm(input_crc8_accum, msg, parity, rxLen);
    }
    

  • Hi Andrea,

    Please ignore using rq. It is not used in the code. So, it is displaying a garbage value.
    Use SNR instead of rq.
    I hope other values are fine when dumped over a period of time.

    Thanks,
    Katta
  • Hi Katta,

    The same happen if I want to see the single SNR of each tone. It display garbage values.

    On the phy_rx.h is write that the values have to range between 0 to 7 for each tone.

    Can you help me?

    Andrea