Hello
Our setup contains a F28M35 pair.
If I intialize both with ZeroConf, they are finding each other.
If I initalize the DC with ZeroConf our SN is joining.
But If I start g3_dc_AM335X_aes_msb_loadng.exe on the DC device there is a "no beacon" error on the SNs discovery step.
./g3_dc_AM335X_aes_msb_loadng.exe -c /dev/ttyUSB1 -B tonemask_fcc2 -F 1
#########################################################################
################# G3 Data Concentrator Version 4.7.0.6 ##############
#########################################################################
Original System Information from device ...
*** SYSTEM INFORMATION ***
Firmware Version.................... 7.6.5.10
Device Type......................... G3
Device Mode......................... MAC
Hardware Revision................... pre Rev. D
Host Port........................... SCI-A
Diag Port........................... SCI-B
Apply RPY........................... no
Auto Mode........................... no
G3 Address Type..................... 0
G3 Long Address..................... ffeeddccbbaa9988
G3 Short Address.................... 0
G3 MAC Segment Length............... 0
DEV_shutDown_Handler: SHUT_DOWN returned success.
Pausing to allow device to reset.
DEV_setSysConfig_Handler: LOAD_SYSTEM_CONFIG returned success.
System Information of device has been set to...
*** SYSTEM INFORMATION ***
Firmware Version.................... 7.6.5.10
Device Type......................... G3
Device Mode......................... MAC
Hardware Revision................... pre Rev. D
Host Port........................... SCI-A
Diag Port........................... SCI-B
Apply RPY........................... no
Auto Mode........................... no
G3 Address Type..................... 0
G3 Long Address..................... ffeeddccbbaa9988
G3 Short Address.................... 0xffff
G3 MAC Segment Length............... 0
The tonemask_fcc2 file contains (fcc full band):
0x21 0x48 0xff 0xff 0xff 0xff 0xff 0xff 0xff 0xff 0xff 0x00 0x00 0x00
A suspect field is G3 Short Address:0xFFFF.
Further the start-net command is blocking on the g3_mgmt_cli_AM335X
Have you any idea what could be wrong here?
Thanks
Roman