Question1: Does AQCTLA2 register have shadow register?
it's clear that AQCTLA register have shadow register which can be configured in AQCTL register.
AQCTLA2 register is just same as AQCTLA register.
It also can control ePWMA action, but source come from T1 or T2 event.
But I can't find anything about individual operation mode in Technical Reference Manual ?
Does it have shadow register? if have, how to updata it?
I guess AQCTLA2 register may be configured by AQCTL.bit.SHDWAQAMODE, AQCTL.bit.LDAQAMODE and AQCTL.bit.LDAQASYC, which is same as AQCTLA.
Question2: where is DCAEVTX or DCBEVTX from in the AQTSRCSEL register.
DCAEVT1, DCBEVT1, DCAEVT2 and DCBEVT2 can be selected as source input of Action Qualifer sunmodule.
Take DCAEVT1 for examle,
where is DCAEVT1 from?
Is it DCAEVT1.force in the figure below ?
if so, i think the following Figure should be modified.