Part Number: TMS320F28377D
Tool/software: TI-RTOS
After load program to the CPU1 of 28377d,I connect the CLA then load symbol to cla,but there is an error up the picture。Click the “run” button an other error “CPU1_CLA1: Can't Run Target CPU: (Error -2060 @ 0x0) Requested operation cannot be done while device is running. Halt the device, and retry the operation. (Emulation package 6.0.504.1)”
In the CMD file I set the L4 and L5as the program space,L0 and L1 as the data space。In the CLA_configClaMemory() the set of the ram is same as the cmd file。
why?
thank you!