Part Number: LAUNCHXL-F28377S
Other Parts Discussed in Thread: CONTROLSUITE, TMS320F28377S
Hello TI community,
I am currently working on the LaunchXL-F28377S TI evaluation board. I am recently having issue with the ADC in 16-bit mode. I have my ADC configured to have SOC triggered from an ePWM. Currently I am using ADCINA2 and ADCINA3 where I have A3 pin grounded. I have a function generator connected for A2. I have an interrupt that is loading 256 samples into an array from the adc results register. In the past I was able to have up 3V of range before clipping (adc value of 65535). I am not sure what happened but I am only able to get up to 1.5V now into ADCINA2. I was wondering if anyone else has had this issue as well.