Part Number: LAUNCHXL-F28377S
Other Parts Discussed in Thread: CONTROLSUITE, C2000WARE
I am trying to run the led_ex1_blinky project from flash on my launchxl-f28377s. I can build and run (debug) the project succesfully using either the CPU1_FLASH or CPU1_RAM configurations. However, when I run (debug) either of them, if I press the reset button on the launchpad or unplug/plug the USB cable, the code will stop running (LED quits blinking).
I can also build and run the Example_28377SLaunchPad project just fine. When I press the reset button while this project is running, it runs after reboot perfectly. So I know the problem is not my dipswitch settings. I tried copying the project properties for this project to my blinky project, but this didn't help.
I have been googling and tweaking the project properties all afternoon to no avail. How do I get this project to run after reboot?
I'm using CCS 7.2.