This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28069: Ramp Generator in Comparator Subsystem: less slope?

Part Number: TMS320F28069


Hi,

we try to implement peak current control with compensation ramp and are using the ramp generator in the CMPSS comparator subsystem.

Datasheet says the reference 12-bit DAC uses the most significant 12 bits of the RAMPSTS countdown register as its input. The low 4 bits of the RAMPSTS countdown register effectively act as a prescale for the falling-ramp rate configurable with RAMPDECVALA.

The problem is that even with the lowest RAMPDECVAL of 1 and the fix prescale of 4 bits, the slope (decrement) is too big.
The RAMPSTS is decremented at SYSCLK, so no chance to reduce the slope further, right?

Any help is appreciated.

Stephan