Other Parts Discussed in Thread: C2000WARE
Tool/software: TI C/C++ Compiler
Hi....
1. I have LAUNCHXL-F28377S so, imported examples of
C:\ti\C2000Ware_1_00_03_00_Software\driverlib\f2837xs\examples\cpu1\cla\CCS\
[cla_ex1_asin] project
2. I selected [CPU1_FLASH] configuration and it worked good.
3. For faster operation I changed option (for running in ram rather than flash)
[build] -> c2000 compiler -> Advanced Options -> Runtime Model Options
=> Run functions from RAM (--ramfunc) -> [on]
4. After ramfunc=on, when i started processor It halts. messaging "No source available for "0x3fe493" "
5. I chaned [2837xS_FLASH_CLA_lnk_cpu1.cmd] file
.cinit : > FLASHB PAGE = 0, ALIGN(4)
.pinit : > FLASHB, PAGE = 0, ALIGN(4)
.binit : > FLASHB, PAGE = 0, ALIGN(4) <= I inserted this line (1/2)
.
.
Cla1Prog : LOAD = FLASHD,
RUN = RAMLS4_5,
table(binit), <= I inserted this line (2/2)
.
.
But It still don't work.
6. What should I do?
7. I anticipate your reply.... thank you
8. When program loading the state is as below
9. My compiler versions are as below ( I tried both of them)