This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28379D: Debug probe error

Part Number: TMS320F28379D


Tool/software: Code Composer Studio

Hi,

I got an error when debug the board using TMS320F28379D MCU.

The console shows the error:    (Error -1044 @ 0x0) The debug probe reported an error.

The error happened in running program after successful loading, (I trird to locate the problem by steps: launch configuration,connetion,loading code and debug. )

Last time I met this error  is because of  the unconnection in pin XRS_N.  

So I want to ask that if the error is still come from this pin whose connection wire quite close to crystal oscillator as shown in picture below.

 

Best regards, DITNY.