Part Number: TMS320F280049
Other Parts Discussed in Thread: ISO1050
Tool/software: Code Composer Studio
We have our clock setup the same as TI's Clocking Circuitry in MCU009A(001)_Sch. Our External Oscillator is not exactly the same but has the same Frequency Stability of 10 ppm. We are using the ISO1050 CAN transceiver. We are reading the CAN messages using two different software, BUSMASTER and PCAN-View via a PEAK USB Connection to the computer. We are running TI's example code can_ex3_external_transmit. BUSMASTER shows errors and PCAN-View does not show any messages. If we lower the Baud Rate from 500k to 250k or 50k, everything works fine. We have a 120 ohm termination resistor between CANH and CANL. This is R11 in our schematic below, even though it is marked Do Not Populate. Also R51 which was used for the internal clock source has been removed.
Thank you in advance for your assistance.
Ian