Hello everyone,
I need modules ePWM1 to ePWM8 to work with symmetric high resolution duty control. All ePWM modules have the same period (TBPRD) but they have different phases (TBPHS).
I am able to obtain the desired behaviour on one ePWM by following the procedure described in the TRM (15.2.4.4.1 High-Resolution Period Configuration). However I would like a bit more information about the initial synchronization at steps 8-9.
As far as I understand:
- The HRPWM will not work if I don't perform this initial configuration
- The HRPWM will not work if this initial configuration is not performed while the timebase clock is running (PCLKCR0[TBCLKSYNC]= 1)
The above is very clear from the manual, but what is not very clear is what I can and cannot do after the initial synchronization. So my question is the following:
If I stop the timebase clock for some time (PCLKCR0[TBCLKSYNC]= 0) and restart it later, will the HRPWM keep performing correctly or does it need to be resynchronized?
Cheers,
Pierre