Part Number: LAUNCHXL-F28027
Other Parts Discussed in Thread: AMC1200
I configured the ADC using c2000 embedded coder support package and connected the A0 pin to the ground and the 3.3V pins in the launchpad. For both readings get a noise. Following image shows the reading when the A0 connected to the 3.3V pin. Why is that happening.
configuration parameters of ADC shown below. ePWM1 frequency is 20kHz. I changed the board, changed the power supply and nothing works.