Other Parts Discussed in Thread: UNIFLASH
I am currently having an issue programming my device after many days of development. The original problem started with an issue programming to flash with a TI SYS/BIOS project where my XDS100 would fail to connect occasionally. Power cycling the board and the emulator was fixing that.
Recently (past day or two) I could not program the device at all. CCS Console would indicate that the Memory Map was successfully initialized, but then after tying to writing to Flash Address 0x00082000 (Sector B) the debug probe reports and error and then it fails. Below is a screen capture of the error window, as well as the console output of the failure.
C28xx_CPU1: GEL Output: Memory Map Initialization Complete C28xx_CPU1: Writing Flash @ Address 0x00082000 of Length 0x00000456 (page 0) C28xx_CPU1: Error: (Error -1135 @ 0xC095) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 7.0.188.0) C28xx_CPU1: Trouble Halting Target CPU: (Error -1044 @ 0x0) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 7.0.188.0) C28xx_CPU1: Error: (Error -1135 @ 0xC095) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 7.0.188.0) C28xx_CPU1: Unable to determine target status after 20 attempts C28xx_CPU1: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging C28xx_CPU1: Error occurred during flash operation: Could not write 0x00000064@Data: target is not connected C28xx_CPU1: Error occurred during flash operation: Could not read 0x00130@Program: target is not connected C28xx_CPU1: PLL configuration status = 0. C28xx_CPU1: Error executing PLL configuration algorithm. Operation cancelled. (0x0) C28xx_CPU1: File Loader: Memory write failed: Unknown error C28xx_CPU1: GEL: File: C:\Users\eweigel\Workspaces\TI_RTOS_F28377S\Debug\TI_RTOS_F28377S.out: Load failed. C28xx_CPU1: Error occurred during flash operation: Could not read register PC: target is not connected C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005F800@Data: target is not connected C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005FC00@Data: target is not connected C28xx_CPU1: Error occurred during flash operation: Could not write 0x00000@Program: target is not connected C28xx_CPU1: Error occurred during flash operation: Cannot enable while the target is disconnected C28xx_CPU1: Error occurred during flash operation: Could not read 0x00000064@Data: target is not connected C28xx_CPU1: Error occurred during flash operation: Could not write 0x00000064@Data: target is not connected C28xx_CPU1: Error occurred during flash operation: Failed to run target while trying to execute pwrite_en.alg C28xx_CPU1: Flash operation timed out waiting for the algorithm to complete. Operation cancelled. C28xx_CPU1: Perform a debugger reset and execute the Boot-ROM code (click on the RESUME button in CCS debug window) before erasing/loading the Flash. If that does not help to perform a successful Flash erase/load, check the Reset cause (RESC) register, NMI shadow flag (NMISHDFLG) register and the Boot-ROM status register for further debug. C28xx_CPU1: Error occurred during flash operation: Could not write 0x00000064@Data: target is not connected C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005D20E@Data: target is not connected C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D20E@Data: target is not connected C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005D20E@Data: target is not connected C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D20E@Data: target is not connected C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005D22E@Data: target is not connected C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005D208@Data: target is not connected C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D208@Data: target is not connected C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005D208@Data: target is not connected C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D208@Data: target is not connected C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005D222@Data: target is not connected C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D222@Data: target is not connected C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D214@Data: target is not connected C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005D20E@Data: target is not connected C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D20E@Data: target is not connected C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D20E@Data: target is not connected C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D222@Data: target is not connected C28xx_CPU1: Error occurred during flash operation: Could not write 0x00000@Program: target is not connected C28xx_CPU1: Error occurred during flash operation: Cannot enable while the target is disconnected C28xx_CPU1: Error occurred during flash operation: Could not read 0x00000064@Data: target is not connected C28xx_CPU1: Error occurred during flash operation: Could not write 0x00000064@Data: target is not connected C28xx_CPU1: Error occurred during flash operation: Failed to run target while trying to execute pwrite_dis.alg C28xx_CPU1: Flash operation timed out waiting for the algorithm to complete. Operation cancelled. C28xx_CPU1: Perform a debugger reset and execute the Boot-ROM code (click on the RESUME button in CCS debug window) before erasing/loading the Flash. If that does not help to perform a successful Flash erase/load, check the Reset cause (RESC) register, NMI shadow flag (NMISHDFLG) register and the Boot-ROM status register for further debug. C28xx_CPU1: Error occurred during flash operation: Could not write 0x00000064@Data: target is not connected C28xx_CPU1: Error occurred during flash operation: Could not write register PC: target is not connected
I tried using UniFlash to see if I could connect to the device and access memory. This worked fine and I was even able to read the sectors of memory in question from the failed CCS debug. Below is a screen capture of several memory reads into flash as well as a successful verify image attempt.
Flash Sector B
Flash Sector G
Verify Image
This was suspicious to me so I loaded up an example project (sci_echoback_cpu01) and to my surprise it loaded fine and stopped at the entry point as shown below.
The emulator disconnects from the device during the InitSysCrtl() routine, and throws an error that it Can't Run Target CPU.
Trying to force the device to wake up fails, so I restarted and assembly stepped into the function until the failure occurs. The failure occurs trying to to the PLLSYSCLKDIV register and throws a can't single step error.
I captured the CPU status registers (ST0 & ST1) as well as the PLL registers before the error, but nothing seemed out of the ordinary.
I think the device might be damaged, but im not sure. Any assistance in identifying the issue or determining the health of the device is greatly appreciated.
Thanks,
Erick