Part Number: TMS320F280049
Hi team,
I have some confusion about the data in following figures.
As the 5.6 figure shown, when the GPIO output low level, the maximum current IOL is 4mA. However, in the 5.1 figure, the range of output current is from -20mA to 20mA, does this mean that the maximum GPIO output current is 20mA?
What's the different of these two variables?
Thanks!
Best Regards/Rayna