This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049: GPIO current limited value

Part Number: TMS320F280049


Hi team,

I have some confusion about the data in following figures.

As the 5.6 figure shown, when the GPIO output low level, the maximum current IOL is 4mA. However, in the 5.1 figure, the range of output current is from -20mA to 20mA, does this mean that the maximum GPIO output current is 20mA?

What's the different of these two variables?

Thanks!

Best Regards/Rayna