Part Number: LAUNCHXL-F28379D
Other Parts Discussed in Thread: C2000WARE
I have SCI-B setup to transmit and receive FIFO I am using SCIA and C successfully with the same setup but B will not write from RXBUF to TXBUF. I have these pin MUX and GMUXs and have linked those ports with a jumper wire:
EALLOW;
GpioCtrlRegs.GPAMUX2.bit.GPIO18 = 2;
GpioCtrlRegs.GPAMUX2.bit.GPIO19 = 2;
GpioCtrlRegs.GPAGMUX2.bit.GPIO18 = 0;
GpioCtrlRegs.GPAGMUX2.bit.GPIO19 = 0;
EDIS;
The txbuf can be written to, but the RXBUF cannot receive that result and is stuck on a value assigned at initialization(76) these are my setup configs
Fifo
void scib_fifo_init()
{ //initializes first in first out buffer for TX and RX
ScibRegs.SCIFFTX.all = 0xE040;
/*Bit 15 = 1: SCI FIFO can resume transmit or receive. SCIRST should be 1 even for Autobaud logic to work.
Bit 14 = 1: SCI FIFO enhancements are enabled
Bit13 = 1: Re-enable transmit FIFO operation
Bit 12-8 = 0: FIFO is empty
Bit 7 = 0: TXFIFO interrupt has not occurred, read-only bit
Bit 6 = 1: Write 0 has no effect on TXFIFINT flag bit, Bit reads back a zero
Bit 5 = 0: TX FIFO interrupt based on TXFFIL match (less than or equal to) is disabled
Bit 4-0 = 0: TXFFIL N/A
*/
ScibRegs.SCIFFRX.all = 0x2044;
/*Bit 15 = 0: Receive FIFO has not overflowed, read-only bit
Bit 14 = 0: Write 0 has no effect on RXFFOVF flag bit, Bit reads back a zero
Bit13 = 1: Re-enable receive FIFO operation
Bit 12-8 = 0: FIFO is empty
Bit 7 = 0: RXFIFO interrupt has not occurred, read-only bit
Bit 6 = 1: Write 1 to clear RXFFINT flag in bit 7
Bit 5 = 0: RX FIFO interrupt based on RXFFIL match (greater than or equal to) will be disabled
Bit 4-0 = 0: RXFFIL N/A
*/
ScibRegs.SCIFFCT.all = 0x0;
/*Bit 15 = 0: Auto-baud detection is not complete. "A","a" character has not been received successfully.
Bit 14 = 0: Write 0 has no effect on ABD flag bit. Bit reads back a zero.
Bit 13 = 0: Disables auto-baud alignment
Bit 12-8 = 0: Reserved
Bit 7-0 = 0: FFTXDLY Reset set pause between character detections on the RX and TX FIFOs 0-> 0 baud delay
*/
}
init
{
// 1 stop bit, No loopback, No parity,8 char bits, async mode,
// idle-line protocol
ScibRegs.SCICCR.all =0x0007;
//SETS CHAR LENGTH TO 8 BIT FOR SCI COMMUNICATIONS
ScibRegs.SCICTL1.all =0x0003;
//Bit 0 = 1: Send received characters to SCIRXEMU and SCIRXBUF
//Bit 1 = 1: Transmitter enabled
ScibRegs.SCICTL2.bit.TXINTENA =1;
//TXINTENA ENABLES TX INTERRUPTS AND IS ASSOCIATED WITH CCTL2 BIT 0
ScibRegs.SCICTL2.bit.RXBKINTENA =1;
//RXBKINTENA ENABLES RX INTERRUPTS AND IS ASSOCIATED WITH CCTL2 BIT 1
ScibRegs.SCIHBAUD.all = 0x0002;
ScibRegs.SCILBAUD.all = 0x008B;
ScibRegs.SCICTL1.all =0x0023;
// Relinquish SCI from Reset