Tool/software: Code Composer Studio
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Hello,
A Mathworks expert has been assigned to assist.
Best regards
Chris
Greetings venkatesh,
I selected ert.tlc in system target file, which enables to choose Boot from Flash option. But i encounter a following error. How to rectify.
### Invoking Target Language Compiler on NewCCSV5pwm.rtw
### Using System Target File: C:\Program Files\MATLAB\MATLAB Production Server\R2015a\rtw\c\ert\ert.tlc
### Loading TLC function libraries
Warning: The data type "int8" uses a word size that is not available on the intended target.
Fixed-point signals using this data type will be put inside a larger word or multi words. When used,
extra software will be generated to force this larger word or multi words to emulate a smaller
word. This emulation is helpful when your prototype target and your final
production target are not the same. If the smaller word size does NOT exist
on the final production target, then consider increasing the word size to
one that is supported.
Warning: The data type "uint8" uses a word size that is not available on the intended target.
.
Warning: The data type "boolean" uses a word size that is not available on the intended target.
### Initial pass through model to cache user defined code
### Caching model source code
### Writing header file NewCCSV5pwm.h
### Writing header file NewCCSV5pwm_types.h
### Writing header file rtwtypes.h
### Writing source file NewCCSV5pwm.c
### Writing header file NewCCSV5pwm_private.h
.
### Writing source file NewCCSV5pwm_data.c
### Writing source file ert_main.c
### TLC code generation complete.
### Evaluating PostCodeGenCommand specified in the model
### Using toolchain: Texas Instruments C2000 Code Generation Tools v5.2.12 | gmake (64-bit Windows)
### Creating 'F:\NewCCSV5pwm_ert_rtw\NewCCSV5pwm.mk' ...
### Using toolchain: Texas Instruments C2000 Code Generation Tools v5.2.12 | gmake (64-bit Windows)
### Creating 'F:\NewCCSV5pwm_ert_rtw\NewCCSV5pwm.mk' ...
### Building 'NewCCSV5pwm': C:\PROGRA~1\MATLAB\MATLAB~1\R2015a\bin\win64\gmake -B -f NewCCSV5pwm.mk all
F:\NewCCSV5pwm_ert_rtw>cd .
F:\NewCCSV5pwm_ert_rtw>if "" == "" (C:\PROGRA~1\MATLAB\MATLAB~1\R2015a\bin\win64\gmake -B -f NewCCSV5pwm.mk all ) else (C:\PROGRA~1\MATLAB\MATLAB~1\R2015a\bin\win64\gmake -B -f NewCCSV5pwm.mk )
C:/ti/ccsv5/tools/compiler/C2000_~1.0/bin/cl2000 --compile_only --large_memory_model --cla_support=cla0 --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/ti/ccsv5/tools/compiler/C2000_~1.0/include" -v28 --float_support=fpu32 -ml -DMODEL=NewCCSV5pwm -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -DONESTEPFCN=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DSTACK_SIZE=512 -DONESTEPFCN=1 -DTERMFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DRT -DSTACK_SIZE=512 -DMODEL=NewCCSV5pwm -DNUMST=1 -DNCSTATES=0 -DHAVESTDIO -IF:/NewCCSV5pwm_ert_rtw -IF:/ -IF:/Matlab DSP -IF: -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/extern/include -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/simulink/include -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/rtw/c/src -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/rtw/c/src/ext_mode/common -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/rtw/c/ert -IC:/MATLAB/SupportPackages/R2015a/texasinstrumentsc2000/toolbox/target/supportpackages/tic2000/inc -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/toolbox/shared/can/src/scanutil -IC:/MATLAB/SupportPackages/R2015a/texasinstrumentsc2000/toolbox/target/supportpackages/tic2000/src -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/toolbox/target/extensions/processor/tic2000/include -IC:/PROGRA~1/MATLAB/MATLAB~1/R2015a/toolbox/rtw/targets/common/can/blocks/tlc_c --output_file="MW_c28xx_board.obj" "F:/NewCCSV5pwm_ert_rtw/MW_c28xx_board.c"
[DSP.]
>> WARNING: more than one source file is specified; option --output_file is ignored
Fatal error: cannot open source file "DSP"
1 catastrophic error detected in the compilation of "DSP".
Compilation terminated.
>> Compilation failure
gmake: *** [MW_c28xx_board.obj] Error 1
F:\NewCCSV5pwm_ert_rtw>echo The make command returned an error of 2
The make command returned an error of 2
F:\NewCCSV5pwm_ert_rtw>An_error_occurred_during_the_call_to_make
'An_error_occurred_during_the_call_to_make' is not recognized as an internal or external command,
operable program or batch file.
### Build procedure for model: 'NewCCSV5pwm' aborted due to an error.
Error(s) encountered while building model "NewCCSV5pwm":
### Failed to generate all binary outputs.
Component: Simulink | Category: Model error
Hi,
There is a path -IF:/Matlab DSP which is part of build and has space in it.
Hence the error: Fatal error: cannot open source file "DSP"
Hi Venkatesh,
Thanks for pointing out, but could you help me to correct it.
Regards,
Logeesan
Hi,
I removed the space between the file name (F:Matlab DSP >> F:MatlabDSP). The build is successful. Thanks for helping me out.
I close this thread.