Part Number: TMS320F280049C
Other Parts Discussed in Thread: C2000WARE
Hi C2K experts,
I have a struct variable in local shared memory.:
typedef struct {
// Inputs
float32 Ref;
float32 Fdbk;
// Internal values
float32 Errn;
float32 Errn1;
float32 Errn2;
// Output values
float32 Out;
float32 Out1;
float32 Out2;
float32 OutPresat;
} CNTL_2P2Z_CLA_C_Vars;
In .cmd file:
CommonDataRAM : > RAMLS2, PAGE = 0
In CLA init.c
MemCfgRegs.LSxCLAPGM.bit.CLAPGM_LS2 = 0U;
MemCfgRegs.LSxMSEL.bit.MSEL_LS2 = 1U;
in cla_task.c
#pragma DATA_SECTION(vloop_vars, "CommonDataRAM");
volatile CNTL_2P2Z_CLA_C_Vars vloop_vars;
__interrupt void Cla1Task1(void)
{
__mdebugstop();
vloop_vars.Ref = 100;
vloop_vars.Fdbk = 92;
normal_routine();
}
However, I saw both of these two variables are 0 in CLA, but correct value in C28.
I don't know if it is normal ?? Or how should I get correct value in CLA ?
C28:
Thanks,