Part Number: TMS320F28377D
Hi,
I am using the F28377D on a customised control board. I used the TI CLB tool to generate a PWM3 at pins GPIO4 and GPIO5 by using CLB overriding option signal using ePWM internal peripherals of PWM1 and PWM2. I have no issue with the CLB tool set up and the code is built with no errors. My concern is that when I am debugging the project I get the below error and I only see the internal peripherals signals PWM1 and PWM2 and I get the below error:
C28xx_CPU1: Error initializing flash programming: Interface returned from dll, but flash is not available on this device.
GPIO4 and GPIO5 are turned on continuously high though but I am not exactly getting the signal I want. I can run different projects with no issues but I am not sure why the control board doesn't work properly with the CLB tool?
F28377D General Control Board - Hardware Description1111.pdf