Part Number: TMS320F28069M
Other Parts Discussed in Thread: C2000WARE, MOTORWARE
Hi,
I have been debugging an issue getting illegal ISR's while trying to merge an application that was written based on C2000Ware/driverlib with a Lab05d based on Motorware/HAL. Got my head tied in knots debugging through the process, one of the places where I got stuck is with the PieVector table, since HAL maintains it's own vector table and C2000ware has it's own.
Debugging and Looking into:
void HAL_enableAdcInts(HAL_Handle handle)
{
HAL_Obj *obj = (HAL_Obj *)handle;
// enable the PIE interrupts associated with the ADC interrupts
PIE_enableAdcInt(obj->pieHandle,ADC_IntNumber_1);
// enable the ADC interrupts
ADC_enableInt(obj->adcHandle,ADC_IntNumber_1);
// enable the cpu interrupt for ADC interrupts
CPU_enableInt(obj->cpuHandle,CPU_IntNumber_10);
return;
} // end of HAL_enableAdcInts() function
void PIE_enableAdcInt(PIE_Handle pieHandle, const ADC_IntNumber_e intNumber)
{
PIE_Obj *pie = (PIE_Obj *)pieHandle;
uint16_t index;
uint16_t setValue;
if(intNumber < ADC_IntNumber_9)
{
index = 9;
setValue = 1 << intNumber;
}
else if(intNumber == ADC_IntNumber_9)
{
index = 0;
setValue = 1 << 5;
}
else
{
index = 0;
setValue = 1 << ((intNumber & 0x07) - 1) ;
}
// set the value
pie->PIEIER_PIEIFR[index].IER |= setValue;
return;
} // end of PIE_enableAdcInt() function
typedef enum
{
ADC_IntNumber_1=0, //!< Denotes ADCINT1
ADC_IntNumber_2, //!< Denotes ADCINT2
ADC_IntNumber_3, //!< Denotes ADCINT3
ADC_IntNumber_4, //!< Denotes ADCINT4
ADC_IntNumber_5, //!< Denotes ADCINT5
ADC_IntNumber_6, //!< Denotes ADCINT6
ADC_IntNumber_7, //!< Denotes ADCINT7
ADC_IntNumber_8, //!< Denotes ADCINT8
ADC_IntNumber_9, //!< Denotes ADCINT9
ADC_IntNumber_1HP, //!< Denotes ADCINT1 High Priority for use with PIE_enableAdcInt() only
ADC_IntNumber_2HP, //!< Denotes ADCINT2 High Priority for use with PIE_enableAdcInt() only
ADC_IntNumber_9HP=0xE //!< Denotes ADCINT9 High Priority for use with PIE_enableAdcInt() only
} ADC_IntNumber_e;
with index = 9 and setValue = 1 in the given context,
the following:
pie->PIEIER_PIEIFR[index].IER |= setValue;
becomes
pie->PIEIER_PIEIFR[9].IER |= 1;
According to spruh18g, 1.7.4 PIE Configuration Registers:
PIEIER9 0x0000 - 0CF2 1 PIE, INT9 Group Enable Register
but, according to Table 1-120. PIE Vector Table:
PIE Group 9 Vectors - MUXed into CPU INT9 are
the SCI-x and CAN-x interrupts.
I can't see clearly how that is working. Most likely, I am missing something here. Can someone please clarify ?
Thanks,
Manu