Hi,
I am running my system clock at 48 MHz which is fixed for my current design. I would like to generate and output a 10 MHz square wave which will act as a clock for one of the external payloads. I suppose bit-banging a GPIO using a timer interrupt may not be a good idea. Will ePWM be able to generate such high frequency or do I have to use some other method to generate? Just need a heads up towards right direction :)
Thanks and Regards,
Ankit