Dear team:
One of my customers didn't reserve GPIO pins for configuring boot mode when designing the PCB board, so he wanted to use the “Zero boot mode select pins” mode to make the device boot to flash.
After reading the TRM, he had the following questions:
1, In which file can these registers be found and configured?
2, Is it possible to test in one of the routines provided by TI?
3, These register configurations are directly written into OTP flash. Once written, will it affect the subsequent re-programming (without modifying the OTP flash)?
Best regards