Other Parts Discussed in Thread: HALCOGEN, TMS570LS0332
Hi,
I am using the TMS570LS0332 with Halcogen 4.4 and CCS6.1. I use the HET module to detect edges to monitor an incoming PWM signal. The signals that are coming in are very noisy (the electrical guys are working on it). But they are noisy enough that they are falsely tripping the edge detection.
Is there a way to configure the threshold that will cause the edge detector to trip? So for instance it can be configured when going low to high to trip at 3.5 or 4 V.
What is the default / current threshold?
Is there any filtering done, or can turned on, for input signals into the HET module?
This is a very urgent issue for me to solve, so any help is greatly appreciated.
Thanks,
David