Other Parts Discussed in Thread: TMS570LS2125
Hi,
Could you teach me the potential voltage level of VIL and VIH for TMS570LS2125?
In the datasheet, VIL(MAX)=0.8V and VIH(MIN)=2.0V are described,
but I think the real thresholds are higher or lower.
The background of this suggestion is that
I must know whether the logic level is clamped and stable when the terminations are shorted.
For example, in case the pull-down termination and the VDD are shorted and the input voltage of the pull-down termination is 0.9V,
if the potential voltage level of VIL is 0.9V,
I can claim the MCU will treat it as low and the logic level is clamped and stable.
Thanks
Nomoto