Other Parts Discussed in Thread: HALCOGEN, TMS570LS20216, TMS570LS20206
Hi
I read all your posts on PIL setup. thanks a lot for your support. Coming to point I am planning to create a PIL setup for TMS570LS20SUSB. For this I have referred your PIL package for RM48.
I have all required MATLAB products R2013a available and I performed all required changes for targetting TMS570.
Below are obstructing me from ending up with successful PIL setup creation.
1. I was left with setting up of Product Hardware Device Type in model configuration settings. For TI it is showing only upto TMS470. which MATLAB version do I need to use for setting device type to TMS570 or Is there any other setting for the same?
2. Which version of CCS will be required for creating PIL setup for TMS570?
3. Which version of Halcogen should be used for creating PIL setup for TMS570? Could you be more precise for performing PIL setup settings required for TMS570. Please share them because setting you have mentioned in RM48 package in not clear.
Thanking you in anticipation.
Regards
Chaitanya P V S