Other Parts Discussed in Thread: SN65HVDA541-Q1
Hello Team,
can you provide a BOM for http://processors.wiki.ti.com/images/f/f5/HDK_FlexrayCanLin_Daughter_Crad.zip please?
Thanks and Best Regards,
Hans-Günter
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: SN65HVDA541-Q1
Hello Team,
can you provide a BOM for http://processors.wiki.ti.com/images/f/f5/HDK_FlexrayCanLin_Daughter_Crad.zip please?
Thanks and Best Regards,
Hans-Günter
Hi Hans-Günter,
pls. find the BOM below.
Best Regards,
Peter
| Item | Quantity | Part | Reference |
| 1 | 1 | 220pF | C20 |
| 2 | 4 | 4n7 | C12,C15,C18,C23 |
| 3 | 1 | 10nF | C3 |
| 4 | 13 | 100nF | C2,C4,C7,C8,C10,C11,C13,C14,C19,C16,C17,C21,C22 |
| 5 | 4 | 10uF | C1,C5,C6,C9 |
| 6 | 1 | 50SQ080 | D1 |
| 7 | 4 | (green) | D2,D3,D4,D5 |
| 8 | 1 | 1N914 | D6 |
| 9 | 1 | VC080526A580 | D7 |
| 10 | 1 | FUSE | F1 |
| 11 | 12 | TP | TP-TX1,TP-TEN1,TP-STB1,TP-RX1,G1,TP-TX2,TP-TEN2,TP-STB2,TP-RX2,G2,G3,G4 |
| 12 | 2 | JP2 | JP1,JP2 |
| 13 | 1 | JP3 | JP3 |
| 14 | 1 | POWER | J1 |
| 15 | 2 | CON2 | J2,J8 |
| 16 | 1 | CON-HDK-J11 | J3 |
| 17 | 4 | CON3 | J4,J5,J6,J9 |
| 18 | 1 | CHINCH_FEMALE | J7 |
| 19 | 1 | DROSSEL I-COMP | L1 |
| 20 | 4 | ACT45B-510-2P | L2,L3,L4,L5 |
| 21 | 2 | 130 | R1,R2 |
| 22 | 15 | 10k | R3,R4,R5,R6,R7,R8,R12,R13,R14,R15,R16,R17,R26,R27,R28 |
| 23 | 2 | 200 | R9,R18 |
| 24 | 4 | 47 | R10,R11,R19,R20 |
| 25 | 2 | 4K7 | R21,R31 |
| 26 | 4 | NP | R22,R23,R32,R33 |
| 27 | 4 | 62 | R24,R25,R34,R35 |
| 28 | 1 | 1k | R29 |
| 29 | 1 | 0 | R30 |
| 30 | 16 | SB2 | SB1,SB2,SB3,SB4,SB5,SB6,SB7,SB8,SB9,SB10,SB11,SB12,SB13,SB14,SB15,SB16 |
| 31 | 1 | POWER-ON | S1 |
| 32 | 2 | TJA1080 | U1,U3 |
| 33 | 2 | TJA1082 | U2,U4 |
| 34 | 2 | SN65HVDA541-Q1 | U5,U7 |
| 35 | 1 | TPIC1021A | U6 |
| 36 | 1 | REG104F4 | VR1 |
| 37 | 1 | REG1117F4 | VR2 |
| 38 | 1 | PCB |