Other Parts Discussed in Thread: HALCOGEN
The _pmuInit_ assembly function in the sys_pmu.asm file generated by HALCoGen 04.03.00 for a RM46L852PGE is the following:
_pmuInit_
stmfd sp!, {r0}
; set control register
mrc p15, #0, r0, c9, c12, #0
orr r0, r0, #(1 << 4) + 6 + 1
mcr p15, #0, r0, c9, c12, #0
; clear flags
mov r0, #0
sub r0, r0, #1
mcr p15, #0, r0, c9, c12, #3
; select counter 0 event
mcr p15, #0, r0, c9, c12, #5 ; select counter
mov r0, #0x11
mcr p15, #0, r0, c9, c13, #1 ; select event
; select counter 1 event
mov r0, #1
mcr p15, #0, r0, c9, c12, #5 ; select counter
mov r0, #0x11
mcr p15, #0, r0, c9, c13, #1 ; select event
; select counter 2 event
mov r0, #2
mcr p15, #0, r0, c9, c12, #5 ; select counter
mov r0, #0x11
mcr p15, #0, r0, c9, c13, #1 ; select event
ldmfd sp!, {r0}
bx lr
.endasmfunc
Looking at the code, I think the section to "select counter 0 event" is not setting the r0 register to the correct value for counter zero before writing to the Performance Counter Selection Register. From single stepping the assembler the code which is supposed to be selecting the counter 0 event ends up writing b00011 to the Performance Counter Selection Register which is not a valid value for the Cortex R4F (valid values are b00000 to b00010 for counters 0 to 2):
The code should be corrected to set r0 to zero to select counter zero:
_pmuInit_
stmfd sp!, {r0}
; set control register
mrc p15, #0, r0, c9, c12, #0
orr r0, r0, #(1 << 4) + 6 + 1
mcr p15, #0, r0, c9, c12, #0
; clear flags
mov r0, #0
sub r0, r0, #1
mcr p15, #0, r0, c9, c12, #3
; select counter 0 event
mov r0, #0
mcr p15, #0, r0, c9, c12, #5 ; select counter
mov r0, #0x11
mcr p15, #0, r0, c9, c13, #1 ; select event
; select counter 1 event
mov r0, #1
mcr p15, #0, r0, c9, c12, #5 ; select counter
mov r0, #0x11
mcr p15, #0, r0, c9, c13, #1 ; select event
; select counter 2 event
mov r0, #2
mcr p15, #0, r0, c9, c12, #5 ; select counter
mov r0, #0x11
mcr p15, #0, r0, c9, c13, #1 ; select event
ldmfd sp!, {r0}
bx lr