I am trying FEE Driver using the TMS570LS3137. The eeprom size of TSM570LS3137 is 64KByte.I am trying use as much as all eeprom size. My source is not using RTOS. is Firmware architecture.
1. use the parameter offset and length of TI_Fee_ReadSync(). but TI_Fee_WriteSync() isn't use the offset and length. I want to use the offset and length to TI_Fee_WriteSync(). if possible, please help me.
2. I can not be set the HALCoGen for using as much as all eeprom size.
2.1. I am trying the 1024byte size the Block Index 1 in FEE Block Configuration tap of HALCoGEN. but does not operated. Is it the limit of Block size?
2.2. Can not be set the one FEE Block index1 to 64Kbyte?
To use the 64Kbyte size, how do i need to set the HALCoGen?