Other Parts Discussed in Thread: TMS570LS1224
Hi Friends,
I am using TMS570LS1224 launchpad, And interfacing MAX6958 7-Segment driver. I2C communication is happening now but I am getting garbage data .
I have 4-digit 7-segment and it always shows 8888 on display.I am not getting why it is happening.I need help.
I tested MAX6958 driver with arduino Uno it is working fine.
here is arduino code:
void setup()
{
//Configure pin I/O
pinMode(motorPin, OUTPUT);
pinMode(potPin, INPUT);
pinMode(earOnePin, OUTPUT);
pinMode(earTwoPin, OUTPUT);
pinMode(earThreePin, OUTPUT);
pinMode(earFourPin, OUTPUT);
pinMode(domeOnePin, OUTPUT);
pinMode(domeTwoPin, OUTPUT);
pinMode(domeThreePin, OUTPUT);
pinMode(domeFourPin, OUTPUT);
//Generate random number for display
randomSeed(analogRead(A1));
//Initialize I2C and MAX6958 chip
Wire.begin();
Wire.beginTransmission(segDisplay);
Wire.write(0x01); //Decode mode command
Wire.write(0x0F); //Decode mode for digits 0-2
Wire.endTransmission(1);
Wire.beginTransmission(segDisplay);
Wire.write(0x02); //Intensity command
Wire.write(0x20); //0x00(min) to 0x3F(max)
Wire.endTransmission(1);
Wire.beginTransmission(segDisplay);
Wire.write(0x03); //Scan limit command
Wire.write(0x03); //Display digits 0-2
Wire.endTransmission(1);
Wire.beginTransmission(segDisplay);
Wire.write(0x04); //Configuration command
Wire.write(0x01); //Normal operation
Wire.endTransmission(1);
while(1)
{
Wire.beginTransmission(segDisplay);
Wire.write(0x20); //Set digit 0
Wire.write(0x0A); //Value 0
Wire.endTransmission(1);
Wire.beginTransmission(segDisplay);
Wire.write(0x21); //Set digit 1
Wire.write(0x01); //Value 1
Wire.endTransmission(1);
}
Wire.beginTransmission(segDisplay);
Wire.write(0x21); //Set digit 1
Wire.write(0x0B); //Value 1
Wire.endTransmission(1);
//Ramp up DC motor (possible issue with boost converter?)
analogWrite(motorPin, 50);
delay(500);
analogWrite(motorPin, 100);
delay(500);
//Set DC motor speed
analogWrite(motorPin, motorSpeed);
}
void loop()
{
//Update currentTime for LED timings
unsigned long currentTime = millis();
//Update ear lights
if(currentTime - earTime >= earInterval)
{
earTime = currentTime;
if(earOne == 1)
{
earOne = 0;
earTwo = 1;
earThree = 0;
earFour = 0;
}
else if(earTwo == 1)
{
earOne = 0;
earTwo = 0;
earThree = 1;
earFour = 0;
}
else if(earThree == 1)
{
earOne = 0;
earTwo = 0;
earThree = 0;
earFour = 1;
}
else
{
earOne = 1;
earTwo = 0;
earThree = 0;
earFour = 0;
}
digitalWrite(earOnePin, earOne);
digitalWrite(earTwoPin, earTwo);
digitalWrite(earThreePin, earThree);
digitalWrite(earFourPin, earFour);
}
//Update dome lights
if(currentTime - domeOneTime >= domeOneInterval)
{
domeOneTime = currentTime;
digitalWrite(domeOnePin, !digitalRead(domeOnePin));
}
if(currentTime - domeTwoTime >= domeTwoInterval)
{
domeTwoTime = currentTime;
digitalWrite(domeTwoPin, !digitalRead(domeTwoPin));
}
if(currentTime - domeThreeTime >= domeThreeInterval)
{
domeThreeTime = currentTime;
digitalWrite(domeThreePin, !digitalRead(domeThreePin));
}
if(currentTime - domeFourTime >= domeFourInterval)
{
domeFourTime = currentTime;
digitalWrite(domeFourPin, !digitalRead(domeFourPin));
}
//Update display numbers
if(currentTime - displayTime >= displayInterval)
{
displayTime = currentTime;
Wire.beginTransmission(segDisplay);
Wire.write(0x20); //Set digit 0
Wire.write((int)random(1,3)); //Random value between 1 and 2
Wire.endTransmission(1);
Wire.beginTransmission(segDisplay);
Wire.write(0x21); //Set digit 1
Wire.write((int)random(0,10)); //Random value between 0 and 9
Wire.endTransmission(1);
}
}
And here is my Launchpad code:
/* USER CODE BEGIN (2) */
#define DATA_COUNT 12
#define Master_Address 0x26
#define Slave_Address 0b0111000
#define num 0x0F
uint8_t TX_Data_Slave[10] = { 0x01,0x07,0x02,0x20,0x03,0x02,0x04,0x23,0x20,0x01};
/* USER CODE END */
void main(void)
{
/* USER CODE BEGIN (3) */
unsigned char data = 0;
int repeat = 0; int delay =0;
///////////////////////////////////////////////////////////////
// Master Transfer Functionality //
///////////////////////////////////////////////////////////////
/* I2C Init as per GUI
* Mode = Master - Transmitter
* baud rate = 100KHz
* Count = 10
* Bit Count = 8bit
*/
// _enable_interrupt_();
i2cInit();
i2cSetMode(i2cREG1, I2C_MASTER);
/* Configure address of Slave to talk to */
i2cSetSlaveAdd(i2cREG1, Slave_Address);
/* Set direction to Transmitter */
/* Note: Optional - It is done in Init */
i2cSetDirection(i2cREG1, I2C_TRANSMITTER);
/* Configure Data count */
/* Note: Optional - It is done in Init, unless user want to change */
i2cSetCount(i2cREG1, DATA_COUNT);
/* Set mode as Master */
// i2cSetMode(i2cREG1, I2C_MASTER);
/* Set Stop after programmed Count */
i2cSetStop(i2cREG1);
// i2cSetSlaveAdd(i2cREG1, Slave_Address);
/* Transmit Start Condition */
i2cSetStart(i2cREG1);
while(1)
{
i2cSendByte(i2cREG1, TX_Data_Slave[data++]);
}
Regards,
Arvind.