We purchased LDRAUnit from Texas Instruments and are using it to analyze our code that will run on the Hercules. I am running Code Composer V6.0 but it looks like LDRAUnit only allows me to select Code Composer V5.0.
Is there a guide on configuring LDRAUnit to use the correct version of Code Composer? According to some LDRAUnit doc I have read I should be able to use a CodeComposer project file to setup the analysis, include file paths, etc...but this option doesn't seem to be available to me.
I was told by LDRA that since we purchased from TI I need to work with TI on configuration.