Other Parts Discussed in Thread: TMS570LS0432
Dear Sir, I can programme bank 0 of TMS570LS0432 with F021 but can programme bank 7.Here is the code:
if ((Fapi_initializeFlashBanks((uint32_t)SYS_CLK_FREQ)) == Fapi_Status_Success){
(void)Fapi_setActiveFlashBank((Fapi_FlashBankType)7);
Fapi_enableEepromBankSectors(0xffff,0xffff);
}
else {
return (1);
}
while( FAPI_CHECK_FSM_READY_BUSY != Fapi_Status_FsmReady );
while( FAPI_GET_FSM_STATUS != Fapi_Status_Success );
while( SizeInBytes > 0) {
Fapi_issueProgrammingCommand(
(uint32_t *)dst,
(uint8_t *)src,
(uint32_t) bytes,
0,
0,
Fapi_AutoEccGeneration);
while( FAPI_CHECK_FSM_READY_BUSY == Fapi_Status_FsmBusy );
// while(FAPI_GET_FSM_STATUS != Fapi_Status_Success);
src += bytes;
dst += bytes;
SizeInBytes -= bytes;
if ( SizeInBytes < 16){ bytes = SizeInBytes; }
}
Please help me.
Thanks!
Arctop