This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How can I get data using i2c? (feat. MPU-6050)

Other Parts Discussed in Thread: TMS570LC4357, HALCOGEN

First, I'm using Hercules Development Kit(TMS570LC4357) and Halcogen+CCS v6.1.3.

And I also use MPU-6050(Gyro+Accel sensor).

I already connect each pin J11(Expansion Connector on backboard)-SPI3NCS2(Alternative pin) to I2C_SDA in sensor,    J11-SPI3NCS3 to I2C_SCL in sensor. (use two bus lines).

And, for power support to MPU-6050, I connect the pin to J11 - GIOA[4](default) pin (because that voltage is 3.3V).

Gnd? absolutely connect!!!

Every single pin is connect perfectly. Because, I can check MPU-6050 sensor is turn on(through LED light on board).

Here is my question.

I try to receive continuous data from MPU-6050. I followed the example in HalCoGen, and configure some resisters setting.

There are examples about I2C, but that is only self-communication.(loop back)

Anyway, I can not catch the f-king continuous data from MPU-6050.

How can i get data from MPU-6050???? And How can i check and see the data???

I need your specific help about this problem.

For reference, HDK is master(address - 0x26), and sensor is slave(address - 0x68) in I2C communication.

Actullay, i wondering all steps are wrong.