Other Parts Discussed in Thread: TMS570LS1227, UNIFLASH
Hello,
I was using the TMS570LS1227 MCU with CCS v5.4 and everything was working fine as I was able to run a motor through a GUI and load code throughout the day. However, suddenly, without changing anything on the board or its connections, I am now seeing the following error message popup:
"CortexR4: A fatal error occurred while attempting to remove the remaining debug state that could not be removed at disconnect. This might have occurred because a breakpoint was set at an address that is no longer valid. This behaviour may be turned off in the "Debug Properties" tab in the Customize dialog under the Option menu."
I've tried resetting the board, CCS, disconnecting and reconnecting everything, as well as testing the connection to the board itself by "Launching target configuration" (which failed to connect) for the appropriate version but none of these seemed to do the trick. I tried changing the Debug configurations as well but it didn't change the result. I wasn't able to find any other solution online. Is there something else I can try?
Thank you for the help.