Hi,
What is the minimum resolution in nano seconds that can be achieved using ePWM module on TMS570LS1227? the VCLK4 is maximum 150MHz so it is 6.6ns?
and also using N2HET?
The maximum clock of N2HET in TMS570LS1227 is supposed to be 160Mhz but the data sheet says VCLK2 can maximum be 100 MHz. So the resolution of timings that can be achieved is 10ns not 6.25ns?