Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HALCOGEN: HALCoGen FREERtos template doesn't allow to set up 1-3 rti compare lines.

Part Number: HALCOGEN

Hi.

I'm using HALCOGEN TMS570LC4357ZWT_FREERTOS template. This template has full control over rti module and doesn't allow to setup 1..3 compare modules, which aren't used by RTOS kernel. I didn't find any clean way to setup any of left compare signals, it cannot be done by user function before because of non-OR expression:

/* Enable the compare 0 interrupt. */
portRTI_SETINTENA_REG = 0x00000001U;

I guess that it can be done in user defined rtos thread but it is not best way. Why HALCOGEN disables 1..3 rti compare signals?