Part Number: TMS570LC4357
Hi,
when my system boots up I am getting Cortex-R5 Core Fatal Bus Error (Group 2 channel 3 from the datasheet) and which is causing my nError pin to become active.
When I get the error, ESM register are
Stat2 = 0x00000008
ErrPinStat = 0x00000000
IntOffstHgh = 0x00000024
I am getting the error when my TI_Fee_init() function accesses Fee_BlockConfiguration[u16LoopIndex].FeeBlockNumber (where u16LoopIndex is 5).
I also get the error when I access Fee_BlockConfiguration memory block using memory browser.
So it seems like accessing memory address 0x00074d80 is resulting in the the error that I am getting.
But other that that, my application is running fine. But I need nError pin to work fine in order to implement TPS65381 nError pin monitoring for safety purposes.
I have tried solutions mentioned in previous threads regarding this error with no success.
I am using code composer studio 6.1.2 with Compiler TI v16.9.4. LTS
on my Flash settings under Debug, Auto ECC Generation and Align program segments to 64-bit memory regions is checked off. and I am using "verify" for Flash verification settings.
Any help regarding this would be appreciated!
Thanks,
Swapnil