This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS1114: Generating an ESM Group 2 event for testing handler

Part Number: TMS570LS1114


What is an easy way in code to cause ESM Group 2 event to test that the ESM Group 2 handler is working? 

  • Hi James,

    You can use CCM-R4F error forcing to generate group 2 ESM error.
  • Hello James,

    Unfortunately, I do not have an immediate advice on this. I believe there are some of the CCM test modes that can cause a lockstep compare error and trigger G2 Ch2 but I am not 100% certain on this at the moment and don't have access to the TRM. I will have to double check and get back with you.
  • I have tried to use the safeTI diagnostics tests to generate an ESM 2 event but no luck. I tried every test available in safeTI for CCMR4. Below is a sample code of one of the tests I tried. Am I doing something wrong here? 

    SL_CCMR4F_FailInfo failInfoCCMR4F;

    retVal = SL_SelfTest_CCMR4F(CCMR4F_SELF_TEST_ERROR_FORCING, TRUE, &failInfoCCMR4F);

    This code is the first thing I run inside of main(). 

    Note, I am running code in real time, not debugger mode. I have a simple counter that increments inside the esm handlers and those get sent to terminal for viewing. This interface works, I am able to track esm1 and esm3 events this way. 

  • Hello James,

    One easy way to generate ESM Group 2 error is to write a wrong key to RTIWDKEY register, or not feed the watchdog (DWWD) within the time window.

    I just tested and ESM2.24 is set. The following is my test code:

    1. enable RTI compare0 INT, and set the RTI compare periods as 200ms

    /* Include Files */

    #include "sys_common.h"

    /* USER CODE BEGIN (1) */

    #include "rti.h"

    #include "esm.h"

    /* USER CODE END */

    /** @fn void main(void)

    *   @brief Application main function

    *   @note This function is empty by default.

    *

    *   This function is called after startup.

    *   The user can use this function to implement the application.

    */

    /* USER CODE BEGIN (2) */

    int ctr = 0;

    /* USER CODE END */

    int main(void)

    {

    /* USER CODE BEGIN (3) */

       _enable_IRQ();

       /* Initialize RTI */

       rtiInit();

       /* Enable RTI compare 0 notification */

       rtiEnableNotification(rtiNOTIFICATION_COMPARE0);

       /* Start counter */

       rtiStartCounter(rtiCOUNTER_BLOCK0);

       /* Initialize and start DWD */

       dwwdInit(Generate_NMI, 4095, Size_100_Percent);

       dwdCounterEnable();

       /* DWD is serviced in the RTI interrupt*/

       /* Delay */

       while(ctr < 5);

       /* Stop Servicing DWD */

       rtiDisableNotification(rtiNOTIFICATION_COMPARE0);

       while(1);

    /* USER CODE END */

       return 0;

    }

    /* USER CODE BEGIN (4) */

    void rtiNotification(uint32 notification)

    {

       ctr++;

       dwdReset();

    }

    /* USER CODE END */