Part Number: TMS570LC4357
Tool/software: Code Composer Studio
Hello,
I have been able to repeatedly compile and launch a debug session with the HDK over the past month.
Sometimes when the computer comes out of hibernation or low power standby, it has trouble connecting to the board.
If I disconnect power to the board, and disconnect and reconnect the USB cable, the connection is usually reestablished.
Sometimes I have needed to completely reboot the computer, and then connection is OK.
But now, the connection continuously fails. There is no method or procedure that causes a successful connection anymore.
Is there a means to reset the drivers for the jtag USB Debug Probe?
I have changed to a new HDK board, a new USB cable, and tried all the different available USB ports, and NOTHING is working anymore!
I go into the Project Properties panel, and check verify for the Texas Instruments XDS100V2 USB Debug Probe, and I get:
This error is generated by TI's USCIF driver or utilities. The value is '-150' (0xffffff6a). The title is 'SC_ERR_FTDI_FAIL'. The explanation is: One of the FTDI driver functions used during configuration returned a invalid status or an error.
Since this error is reported for different HDK hardware, different USB cables, and different USB ports, I primarily suspect it is due to a fault in a driver that needs updated.
Please advise on the best way to update or repair drivers for this functionality, please help provide a method to reliably enable connection for loading/starting a debug session on the HDK.
Thank You,
-Joseph