Part Number: TMS570LC4357
Other Parts Discussed in Thread: HALCOGEN
Tool/software: Code Composer Studio
Hi community,
Recently I am working on the UART boot loader on TMS570LC4357. I found a example here https://e2e.ti.com/support/microcontrollers/hercules/f/312/p/699892/2605850?tisearch=e2e-sitesearch&keymatch=TMS570LC4357%20UART%20bootloader#2605850
here is the bootloader preject.7180.TMS570LC4357_UART_Boot.rar
The example boot loader works fine. But, when execution jumps to the applications, the prefetchEntry loops forever.
JumpAddress = (uint32_t)APP_START_ADDRESS; // #define APP_START_ADDRESS 0x00200100
((void (*)(void))JumpAddress)();
I try to modify the link file of the application projects, but prefetchEntry loops all the same. Are there some manuals guiding to modify the link file both bootlaoder and application project?
Here are my application projects, one with FreeRTOS and the other without.
7206.TMS570LC_TestWithFreeRTOS.rar
HalCoGen version is 4.07.01, those projects are tested with hercules HDK