Tool/software: Linux
I use a 941 chip ,and have some questions
1. when cpu have no mipi output, some of our board cannot communication with the remote chip with back channel. I2C & remote GPIO not work.(the ratio is 20%),when mipi output is ready, all of them can use back channel. so when cpu have no output I try to use internal clock and enable test pattern to use i2c to control the remote chip, It also work. so to use back channel, must have video data on fpd?
2.when I use internal clock on&off test pattern will trigger a INTB interrupt(I set the 0xC6=0x41),but on UB947 on/off test pattern will not trigger HPD, they are different? to avoid this interrupt I try to set 0xC6 =0x00 when
I enable&disable test pattern,but the interrput still occur, It seems I can't mask it.why?
3, I set REM_INTB_CTRL 0x30 = 0x0A, but re_intb pin still have a falling edge when remote deserializer have interrupt, so the config means GPIO pins will mirror the re_intb pin, and re_intb still work?
4. in 2:2 mode, once one port have locked a link, then another port locked a link will not trigger a HPD interrupt. Can 941 to make port0/port1 HPD independent?
Thanks.
B&R
Enson Liu