Other Parts Discussed in Thread: HALCOGEN
Hi Ki,
1.
Thank you for excluding the connection as a problem.
Following your post, disabled the auto run, reached the entry point, from here stepping “F5” or “F6” is jumping to reset. Can’t step through until (2).
Now, the next step would be to disable the WDT.
Possible way:
http://www.ti.com/lit/ug/slau132t/slau132t.pdf
page 78, option: --cinit_hold_wdt
2.
Added –cinit_hold_wdt=on flag to the linker:
rror #10427-D: The symbol "WDTCTL_SYM" is unresolved. This symbol is required when --cinit_hold_wdt=on is used. The issue is mostly likely thatyour device does not support holding the watchdog timer when performing C auto initialization.
Then found the symbol:
the preprocessor __ARM_ARCH macro, on compiler:
on page 40: -mv7r4, should have been set.
Do you have a better alternative?
--
Kind regards,
Alexander