Hello Together,
i have a TMDXTMS570LS31HDK and I want to run the "N2HET PWM Example" on it. If I use the complete Project Example (provided here http://processors.wiki.ti.com/index.php/Category:TMS570) it works fine, but if i try to build the Project by my self with HALCoGen and CSS the Code which is generated is a bit different and it does not work on the development board.
Do you have any idea/hint what I am doing wrong?
If you need further information please ask :)
HALCoGen: 03.06.00
Code Composer Studio: 5.4.00091
ARM Compiler: 5.1
Faithfully
MaTT