Other Parts Discussed in Thread: HALCOGEN
Hi,Ti:
My project is running ok when there are not "safety init".
But ,after I enable "safety init" with HAL Code Generator,My project will suspend at sys_startup.c.
It stop at there ,behind with red mark.
Please tell me why?
How can I do ?
if ((esmREG->SR1[2]) != 0U)
{
/* USER CODE BEGIN (24) */
/* USER CODE END */
/*SAFETYMCUSW 5 C MR:NA <APPROVED> "for(;;) can be removed by adding "# if 0" and "# endif" in the user codes above and below" */
/*SAFETYMCUSW 26 S MR:NA <APPROVED> "for(;;) can be removed by adding "# if 0" and "# endif" in the user codes above and below" */
/*SAFETYMCUSW 28 D MR:NA <APPROVED> "for(;;) can be removed by adding "# if 0" and "# endif" in the user codes above and below" */
for(;;)
{
}/* Wait */